You use the search tool to find objects or properties that have the name or other property in common. You then mass create identical trend logs for these objects instead of creating the trend logs one by one for each object or property.
In WorkStation, in the Search box, type the name or the property that the objects have in common.
Click the Search button
In the Search view, select the objects or properties you want to create trend logs for.
On the File menu, point to New and then click Trend .
In the Create Object wizard, in the object type list, select the trend log you want to create.
In the Prefix box, type a label that is added in front of the name of the trend logs.
In the Suffix box, type a label that is added after the name of the trend logs.
In the Description box, type a description for the trend logs.
In the Destination box, enter the destination where you want to create the trend logs. If you use A different folder, relative to the selected object , this destination applies to the first object in the list, and its path works as a pattern for the relative path that is applied to all the remaining objects.
If the specified relative path pattern leads to an unavailable position for any of the objects in the list, Next and Create are disabled.
Click Next .
See the trend log procedures for detailed information on how to create and set up your specific trend log type:
Więcej informacji zawiera Creating a Change of Value Trend Log .
Więcej informacji zawiera Creating an Interval Trend Log .
Więcej informacji zawiera Creating a Variable Triggered Trend Log .