earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Тренды
Версия продукта: 2024, 7.0
02.12.2024

Mass Creating Trend Logs

You use the mass create feature to create identical trend logs for different objects, instead of creating the trend logs one by one.

Показать больше
action_close

You use the mass create feature to create multiple identical alarms or trend logs for different objects, instead of creating the alarms or trend logs one by one. From trend logs, you can mass create extended trend logs.

The main principle in the EcoStruxure Building Operation software is that what you can do from one object or property, you can mass create from a number of selected objects or properties on a one to one basis. For example, you have seven objects that you want to monitor with seven interval trend logs. By selecting the objects and starting the ordinary New Object wizard, you configure a generic interval trend log template. When finishing the wizard seven identical interval trend logs that monitor individual objects are automatically created.

 
action_zoom_plus_stroke Mass creating identical trend logs from different variables.
Рисунок: Mass creating identical trend logs from different variables.

Object or Property Variable Type

In the EcoStruxure Building Operation database, you can create alarms or trend logs that are suitable for the variable type you have selected.

Более подробную информацию см. Object or Property Variable Type .

Suffix and Prefix

When you mass create objects you can specify a prefix and suffix that are added to the created object name. The prefix is added before the name and the suffix is added after.

Более подробную информацию см. Suffix and Prefix .

Mass Create Unit Management

You can only mass create alarms with identical units or no unit. When you mass create trend logs, each trend log gets the same unit as the logged variable.

Более подробную информацию см. Mass Create Unit Management .

Mass Create from Properties with the Search Method

Mass creating can be performed by either selecting objects in the object list or selecting the objects or properties in a search result list. Using the search result list is very convenient if you want to monitor a number of properties located in different devices or folders. For example, you want to create enumeration alarms that monitor the reliability property on several I/O points. The I/O points are located on several field servers. By performing a search for the reliability property you can select the points that you want to monitor in the search result list.

Mass Create Path Options

You have three options when deciding where to create new alarms, trend logs, and extended trend logs:

  • The same folder as each selected object

  • A different folder, relative to the path of each selected object

  • A single folder for all created objects

To mass create trend logs
  1. In WorkStation, in the List View, select the objects that you want to create trend logs for.

  2. On the File menu, point to New and then click Trend .

  3. In the Create Object wizard, in the object type list, select the trend log you want to create.

  4. In the Prefix box, type a label that is added in front of the name of the trend logs.

  5. In the Suffix box, type a label that is added after the name of the trend logs.

  6. In the Description box, type a description for the trend logs.

  7. In the Destination box, enter the destination where you want to create the trend logs. If you use A different folder, relative to the selected object , this destination applies to the first object in the list, and its path works as a pattern for the relative path that is applied to all the remaining objects.

    Примечание

    If the specified relative path pattern leads to an unavailable position for any of the objects in the list, Next and Create are disabled.

  8. Click Next

See the trend log procedures for detailed information on how to create and set up your specific trend log type:

  • Mass Create
  • Mass Create Unit Management
  • Mass Create Path Options
  • Mass Creating Trend Logs Using the Search Method
  • Create Object Dialog – Naming the Object Page
  • Object or Property Variable Type
  • Trends Overview
  • Creating a Change of Value Trend Log
  • Creating an Interval Trend Log
  • Creating a Variable Triggered Trend Log
  • Cannot Mass Create Trend Logs or Alarms