earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-P-3, AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 7.0, 7.1
10/30/2025

Matching Text String Alarms

​A matching text string alarm evaluates if the monitored value equals the given text strings.

Note:
  • The text string is case sensitive and must be written exactly as the monitored variable text output.

  • Wildcards cannot be used in the text string.

For example, a script program inside a b3 Continuum system generates text strings that you want to monitor. You configure the matching text string alarm to trigger an alarm when a certain string is sent from the device.

Matching text string alarms can be configured using shunt variable and time delay. For more information, see Alarm Functions .

  • Alarm Types
  • Alarms Overview
  • Alarm Functions
  • Matching Text String Alarm Properties – Basic Tab
  • Creating a Matching Text String Alarm