earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmas
Versión del producto: 2.0, 2.1, 3.0, 3.1
18/05/2018

Matching Text String Alarms

​A matching text string alarm evaluates if the monitored value equals the given text strings.

Aviso
  • The text string is case sensitive and must be written exactly as the monitored variable text output.

  • Wildcards cannot be used in the text string.

For example, a script program inside a b3 Continuum system generates text strings that you want to monitor. You configure the matching text string alarm to trigger an alarm when a certain string is sent from the device.

Matching text string alarms can be configured using shunt variable and time delay. Para obtener más información, consulte Alarm Functions .

  • Alarm Types
  • Alarms Overview
  • Alarm Functions
  • Matching Text String Alarm Properties – Basic Tab
  • Creating a Matching Text String Alarm