Funzionalità: Allarmi
Versione del prodotto: 3.2, 3.3, 2022
15/10/2020

Matching Text String Alarms

​A matching text string alarm evaluates if the monitored value equals the given text strings.

Avviso
  • The text string is case sensitive and must be written exactly as the monitored variable text output.

  • Wildcards cannot be used in the text string.

For example, a script program inside a b3 Continuum system generates text strings that you want to monitor. You configure the matching text string alarm to trigger an alarm when a certain string is sent from the device.

Matching text string alarms can be configured using shunt variable and time delay. Per maggior informazioni, consulta Alarm Functions .

  • Alarm Types
  • Alarms Overview
  • Alarm Functions
  • Matching Text String Alarm Properties – Basic Tab
  • Creating a Matching Text String Alarm