earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 趋势
产品版本: 2.0, 2.1, 3.0, 3.1
2018/12/13

Meter Change History Dialog Box

Use the Meter Change History dialog box to display all meter changes together with the replaced meters settings.

注释:
  • The Meter Change History dialog box only applies to meter trend log.

 
action_zoom_plus_stroke Meter change history dialog box
图: Meter change history dialog box

表格: Meter Change History Dialog Box

Component

Description

End time

​​Displays the time when the old meter was replaced.

End value

​Displays the value the old meter had when it was replaced.

Unit

Displays the unit of the old meter.

Start time

​Displays the time when the new meter was installed.

Start value

​Displays the value of the new meter when it was installed.

Meter constant

​Displays the constant of the new meter. If the meter counts in kilo (10 3 ), the constant is 1000.

Min value

​Displays the first value of the new meter after roll-over.

Max value

​Displays the last value of the new meter before roll-over.

  • 仪表功能
  • Meter Trend Log Calculation Fails