earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-L, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Localización
Versión del producto: 1.9
12/10/2017

Metric Prefixes

​​WorkStation supports the metric prefix range from yocta (10 -24 ) to yotta (10 24 ). The use of a prefix is optional and is defined together with the unit.

10n

Decimal

Prefix

Symbol

10 -24

0.000 000 000 000 000 000 000 001

yocto

y

10 -21

0.000 000 000 000 000 000 001

zepto

z

10 -18

0.000 000 000 000 000 001

atto

a

10 -15

0.000 000 000 000 001

femto

f

10 -12

0.000 000 000 001

pico

p

10 -9

0.000 000 001

nano

n

10 -6

0.000 001

micro

µ

10 -3

0.001

milli

m

10 -2

0.01

centi

c

10 -1

0.1

deci

d

-

-

-

-

10 1

10

deca

da

10 2

100

hecto

h

10 3

1 000

kilo

K

10 6

1 000 000

mega

M

10 9

1 000 000 000

giga

G

10 12

1 000 000 000 000

tera

T

10 15

1 000 000 000 000 000

peta

P

10 18

1 000 000 000 000 000 000

exa

E

10 21

1 000 000 000 000 000 000 000

zetta

Z

10 24

1 000 000 000 000 000 000 000 000

yotta

Y

If a value has, for example, kilo as prefix, it is presented in WorkStation with the k-prefix independent of the number of decimals. When conversion of a unit that has a prefix, WorkStation removes the prefix and presents the converted value in the operating system settings default measurement unit without the prefix.

For example, A value of 15 is created with the unit set to meter and with the milli prefix (10 -3 ), which gives 15 millimeter. A WorkStation on an operating system with US Customary converts the value to 0.016 yards. This is because of the milli prefix (10 -3 ) is removed and the Building Operation US customary default length unit is yard.

  • Value Presentation
  • Regional and Language Overview
  • Unit Selection Dialog Box
  • Configuring Regional Settings
  • Adding or Changing a Unit and Prefix for a Value