earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 1.8, 1.9
4/20/2017

Mass Backup

Mass backup is a method of performing a manual, simultaneous backup of all the SmartStruxure servers in the network, which is useful for capturing data at a critical point, such as prior to an upgrade. You can choose which SmartStruxure servers you want to back up along with the type of data for each.

In smaller installations, a server group may include an Enterprise Server and one or more SmartStruxure server devices. In larger installations, multiple server groups may include an Enterprise Server with a distinct set of SmartStruxure server devices. In either case, the Enterprise Server is the hierarchical top SmartStruxure server with one or more SmartStruxure server devices.

 
action_zoom_plus_stroke Mass backup of an Enterprise Server and SmartStruxure server devices
Figure: Mass backup of an Enterprise Server and SmartStruxure server devices

You log on to the Enterprise Server to create a mass backup. For more information, see Backup Options Dialog Box .

  • Manual Backups
  • Backup
  • Synchronized Backups
  • Backup Options Dialog Box