earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 2023
16/12/2022

Mass Backup

Mass backup is a method of performing a manual, simultaneous backup of all the EcoStruxure BMS servers in the network, which is useful for capturing data at a critical point, such as prior to an upgrade. You can choose which EcoStruxure BMS servers you want to back up along with the type of data for each.

In smaller installations, a server group may include an Enterprise Server and one or more automation servers. In larger installations, multiple server groups may include an Enterprise Server with a distinct set of automation servers.

In an EcoStruxure BMS that has an Enterprise Central with attached Enterprise Servers, you can do a mass backup of all the Enterprise Servers.

 
action_zoom_plus_stroke Mass backup of an Enterprise Server and automation servers
Figure : Mass backup of an Enterprise Server and automation servers

You log on to the Enterprise Server to create a mass backup. Pour plus d'informations, voir Backup Options Dialog Box .

  • Manual Backups
  • Backup
  • Synchronized Backups
  • Backup Options Dialog Box