earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1
2018/6/26

Mass Backup

Mass backup is a method of performing a manual, simultaneous backup of all the EcoStruxure BMS servers in the network, which is useful for capturing data at a critical point, such as prior to an upgrade. You can choose which EcoStruxure BMS servers you want to back up along with the type of data for each.

In smaller installations, a server group may include an Enterprise Server and one or more SmartX servers. In larger installations, multiple server groups may include an Enterprise Server with a distinct set of SmartX servers.

In an EcoStruxure BMS that has an Enterprise Central with attached Enterprise Servers, you can do a mass backup of all the Enterprise Servers.

 
action_zoom_plus_stroke Mass backup of an Enterprise Server and SmartX servers
图: Mass backup of an Enterprise Server and SmartX servers

You log on to the Enterprise Server to create a mass backup. 有关更多信息,请参阅 Backup Options Dialog Box .

  • Manual Backups
  • Backup
  • Synchronized Backups
  • Backup Options Dialog Box