earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 2.0, 2.1, 3.0, 3.1
03/12/2019

Mass Edit

Use mass edit when you want to change several property values or rename several objects at a time.

You can change several property values at a time, for example, when you want to change all setpoints from 22 to 20. Para obtener más información, consulte Mass Editing Objects .

 
action_zoom_plus_stroke Multi editing
Figura: Multi editing

The objects do not need to be of the same type to be mass edited. However, the properties you want to edit have to be of the same type.

You can mass rename all objects that are possible to move. For example, you can rename alarms but not properties.

You can rename the objects one by one. You can also copy row-separated text from a file, such as an MS Excel file, and paste it to rename several rows in one single operation. When you paste, the copied text is pasted from the row you have clicked and down in the list. If the copied text is longer than the number of rows, pasting stops at the last row.

Para obtener más información, consulte Mass Renaming Objects  .

Para obtener más información, consulte Mass Renaming Objects Using Copy and Paste  .

When you hover over the names in the Name column, the full path of the object is displayed.

You can mass change the units of objects in a search result. Para obtener más información, consulte Mass Changing Units .

  • EcoStruxure Building Operation Objects
  • Mass Editing Objects
  • Mass Renaming Objects 
  • Mass Renaming Objects Using Copy and Paste 
  • Mass Changing Units
  • Rename Dialog Box
  • Object Names
  • Object Properties