Use the Basic tab to view or edit the basic properties of a multistate alarm.
Component |
Description |
Alarm state |
Displays the present state of the alarm. Für weitere Informationen siehe Alarm States . |
Basic evaluation state |
Displays False when the alarm is in its normal state. |
Evaluation state |
Displays the present evaluation state of the alarm. For example, Upper limit alarm is displayed when the monitored value reaches the upper alarm limit. |
Disabled cause |
Displays the cause for the alarm being disabled:
|
Monitored variable |
Enter the path to the variable that is monitored by the alarm. |
![]() |
Click to create a new alarm trigger item, either an integer or range value. Für weitere Informationen siehe Create Object Dialog – Naming the Object Page . |
![]() |
Click to edit the alarm trigger item. Für weitere Informationen siehe Alarm Trigger Properties – Range Tab . Für weitere Informationen siehe Alarm Trigger Properties – Value tab . |
![]() |
Click to remove an alarm trigger item. |
Reset delay (s) |
Enter the time, in seconds, the alarm has to be within the reset criteria before the alarm state is changed from alarm to reset. Für weitere Informationen siehe Time Delay . |
Alarm delay (s) |
Enter the time, in seconds, the alarm has to be within the alarm criteria before the alarm is triggered. Für weitere Informationen siehe Time Delay . |
Shunt variable 1 |
Enter the shunt variable that is used to enable or disable the alarm. Für weitere Informationen siehe Shunt Variables . |
Invert shunt value 1 |
Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. Für weitere Informationen siehe Shunt Variables . |
Shunt operator |
Select AND or OR to add logic between the first and the second shunt variable. Für weitere Informationen siehe Shunt Variables . |
Shunt variable 2 |
Enter the second shunt variable that is used to enable or disable the alarm. Für weitere Informationen siehe Shunt Variables . |
Invert shunt value 2 |
Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. Für weitere Informationen siehe Shunt Variables . |