earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2.0, 2.1, 3.0, 3.1
2018/5/18

Multistate Alarms

​The multistate alarm monitors a variable and triggers the alarm if the variable is between the configured alarm range or equal to a single value. You can add several ranges or single values to trigger the alarm.

注释:
  • The trigger values and the monitored variable must be integer.

 
action_zoom_plus_stroke Multistate alarm triggers an alarm when the monitored variable goes inside the configured range or a single value.
图: Multistate alarm triggers an alarm when the monitored variable goes inside the configured range or a single value.

For example, you have a function block program with an output variable that generates integer values for different states. By using a multistate alarm, you can monitor a specific value or several value ranges.

You can configure multistate alarms using shunt variable and time delay. 有关更多信息,请参阅 Alarm Functions .

  • Alarm Types
  • Alarms Overview
  • Alarm Functions
  • Multistate Alarm Properties – Basic Tab
  • Creating a Multistate Alarm