earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool, WebStation
Funktionaliteter: Tidsscheman
Produktversion: 3.2, 3.3, 2022
2021-07-20

Multistate Schedules

A multistate schedule controls a device that has output states based on integers or positive whole numbers including zero.

For example, you can create a multistate weekly schedule that is bound to a multistate value to control an air handler unit in an office building. To regulate the air circulation Monday through Friday from 08:00 to 17:00, you can set the value to 2 (occupied) when the schedule is active and 1 (unoccupied) when the schedule is inactive.

 
action_zoom_plus_stroke Multistate Schedule
Figur: Multistate Schedule
  • Schedule Types
  • Creating a Multistate Schedule
  • Modifying a Schedule Using the Text View
  • Modifying a Schedule Using the Graphic View