earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Device Administrator, Enterprise Central, Enterprise Server, ​License Administrator, ​License Server, AS-P, Virtual Project Servers, WebReports, Software Administrator
Functionalities: Basic Functionality
Product version: 2.0, 2.1, 3.0, 3.1
6/26/2018

System Backup

Before upgrading the system, it is strongly recommended that you archive the historical data and back up the EcoStruxure BMS servers to preserve the current data and configurations. If you plan to upgrade WebReports, be sure to back up the Reports database in SQL Server.

The following diagram describes the recommended steps for archiving and backing up a multi-server system running EcoStruxure Building Operation software.

 
action_zoom_plus_stroke System archive and backup process overview
Figure: System archive and backup process overview

Table: System Archive and Backup Process Overview

Step

Procedure

Description

1

Archive system data

Perform a manual archive of the system historical data in the Enterprise Server or Enterprise Central. (Archiving is not on SmartX servers.) For more information, see Manually Creating an Archive .

2

Back up current EcoStruxure BMS servers

Create an All data backup for the Enterprise Central, Enterprise Server, and each SmartX server. The backups do not need to follow any particular order. For more information, see Backing Up EcoStruxure BMS Servers Manually .

3

Save backup sets to an external location

Save the Enterprise Central, Enterprise Server, and SmartX server backup sets (.xbk) to a safe location on a file system that is external to the Entrerprise Central or Enterprise Server. For more information, see Backup Set Storage and Protection .

4

Back up current Reports database

For systems that include a Reports Server, back up the WebReports database. For more information, see Backing Up the WebReports Database .

You can also back up the Reports database folder to another location on the file system (not the default source location in the C:\Program Files\ directory).

  • System Upgrade Overview
  • Backup
  • Manually Creating an Archive
  • Checking the Backup Status of an EcoStruxure BMS Server
  • Backup Set Storage and Protection
  • Backing Up EcoStruxure BMS Servers Manually
  • Backing Up the WebReports Database
  • Restore