earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-L, AS-B, Device Administrator, Enterprise Central, Enterprise Server, License Administrator, License Server, AS-P, Project Configuration Tool, WebReports, Software Administrator
Funcionalidades: Funcionalidad básica
Versión del producto: 2.0, 2.1, 3.0, 3.1
26/06/2018

System Backup

Before upgrading the system, it is strongly recommended that you archive the historical data and back up the EcoStruxure BMS servers to preserve the current data and configurations. If you plan to upgrade WebReports, be sure to back up the Reports database in SQL Server.

The following diagram describes the recommended steps for archiving and backing up a multi-server system running EcoStruxure Building Operation software.

 
action_zoom_plus_stroke System archive and backup process overview
Figura: System archive and backup process overview

Tabla: System Archive and Backup Process Overview

Step

Procedure

Description

1

Archive system data

Perform a manual archive of the system historical data in the Enterprise Server or Enterprise Central. (Archiving is not on SmartX servers.) Para obtener más información, consulte Manually Creating an Archive .

2

Back up current EcoStruxure BMS servers

Create an All data backup for the Enterprise Central, Enterprise Server, and each SmartX server. The backups do not need to follow any particular order. Para obtener más información, consulte Backing Up EcoStruxure BMS Servers Manually .

3

Save backup sets to an external location

Save the Enterprise Central, Enterprise Server, and SmartX server backup sets (.xbk) to a safe location on a file system that is external to the Entrerprise Central or Enterprise Server. Para obtener más información, consulte Backup Set Storage and Protection .

4

Back up current Reports database

For systems that include a Reports Server, back up the WebReports database. Para obtener más información, consulte Backing Up the WebReports Database .

You can also back up the Reports database folder to another location on the file system (not the default source location in the C:\Program Files\ directory).

  • System Upgrade Overview
  • Backup
  • Manually Creating an Archive
  • Checking the Backup Status of an EcoStruxure BMS Server
  • Backup Set Storage and Protection
  • Backing Up EcoStruxure BMS Servers Manually
  • Backing Up the WebReports Database
  • Restore