earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: License Administrator, License Server
Funkcje: Zarządzanie licencją
Wersja produktu: 3.2, 3.3, 2022, 2023
2020-07-15

EcoStruxure Building Operation Software License Return

When you return an EcoStruxure Building Operation software license, the license is transferred from the License Server back to the License Activation Server.

The returned license is not available is not available for the WorkStation or Enterprise Server to activate.

When a license is returned, all the licenses that were activated in the same session are also returned. For example, if seven licenses are activated in the same activation transaction, a single license cannot be returned to the License Activation Server.

To activate the returned licenses again, use the entitlement ID that contains the returned licenses.

This flow describes the return transaction of licenses from a License Server to the License Activation Server.

 
action_zoom_plus_stroke Returning a license from License Server to the License Activation Server
Rysunek: Returning a license from License Server to the License Activation Server

Tabela: Returning Licenses from License Server to the License Activation Server

Number

Description

1

In the License Administrator, select the licenses to return.

2

The License Administrator returns the licenses to the License Activation Server.

Uwaga
  • All licenses that were activated in same transaction are returned to the License Activation Server.

  • EcoStruxure Building Operation Software License Maintenance
  • Licenses View Icons
  • Returning EcoStruxure Building Operation Software Demo Licenses Using License Administrator