earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: ​License Administrator, ​License Server
功能: 许可证管理
产品版本: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1
2015/5/28

Network License Return

To return a network license means that a license is transferred from the License Server back to the License Activation Server. A returned network license, located on the License Activation Server, is not available for the WorkStation or Enterprise Server to check out.

When returning a license, all the licenses that were activated in the same session are also returned. For example, if seven licenses are activated in the same activation transaction, a single license cannot be returned to the License Activation Server.

To once again activate the returned licenses, use the entitlement ID that contains the returned licenses.

This workflow describes the return transaction of licenses from a License Server to the License Activation Server.

 
action_zoom_plus_stroke Returning a license from License Server to the License Activation Server
图: Returning a license from License Server to the License Activation Server

表格: Returning Licenses from License Server to the License Activation Server

Number

Description

1

In the License Administrator, select the licenses to return.

2

The License Administrator returns the licenses to the License Activation Server.

注释:
  • All licenses that were activated in same transaction are returned to the License Activation Server.

  • License Maintenance
  • Service and Maintenance
  • Licenses View Icons
  • Removing a Local License or Returning a Network License