earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2.0, 2.1, 3.0, 3.1
5/5/2021

Create Alarm Wizard – Attachment Page

Use the Attachment page to add attachments to an alarm or an alarm decoration.

 
action_zoom_plus_stroke Attachment page
Figure: Attachment page

Table: Attachment Page or Tab

Property

Description

 
action_zoom_plus_stroke

Add attachment

Click to add an attachment to the alarm decoration rule. For more information, see Alarm Attachments

 
action_zoom_plus_stroke

Remove attachment

Click to remove the selected attachment from the alarm decoration rule.

 
action_zoom_plus_stroke

Navigate to 

Click to open the attachment that is selected in the attachment list.

Type

View the object type of the attachment.

Name

View the name of the attachment.

Display on alarm

Select to display the attachment when the alarm is going from Normal to Alarm state. 

Path

View the path of the attachment.

  • Alarm Functions
  • Alarm Decoration
  • Create Object Wizard – Naming the Object Page
  • Create Alarm Wizard – Presentation Page
  • Create Alarm Wizard – User Action Page