Use the Attachment page to add attachments to an alarm or an alarm decoration.
Property |
Description |
![]() |
Add attachment Click to add an attachment to the alarm decoration rule. Pour plus d'informations, voir Pièces jointes à une alarme . |
![]() |
Remove attachment Click to remove the selected attachment from the alarm decoration rule. |
![]() |
Navigate to Click to open the attachment that is selected in the attachment list. |
Type |
View the object type of the attachment. |
Name |
View the name of the attachment. |
Display on alarm |
Select to display the attachment when the alarm is going from Normal to Alarm state. |
Path |
View the path of the attachment. |