Use the Attachment page to add attachments to an alarm or an alarm decoration.
Property |
Description |
|
Add attachment Click to add an attachment to the alarm decoration rule. Mer information finns i Alarm Attachments . |
|
Remove attachment Click to remove the selected attachment from the alarm decoration rule. |
|
Navigate to Click to open the attachment that is selected in the attachment list. |
Type |
View the object type of the attachment. |
Name |
View the name of the attachment. |
Display on alarm |
Select to display the attachment when the alarm is going from Normal to Alarm state. |
Path |
View the path of the attachment. |