earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2024, 7.0
2024/12/3

Create Alarm Wizard – Attachment Page

Use the Attachment page to add attachments to an alarm or an alarm decoration.

 
action_zoom_plus_stroke Attachment page
图: Attachment page

表格: Attachment Page or Tab

Property

Description

 
action_zoom_plus_stroke

Add attachment

Click to add an attachment to the alarm decoration rule. 有关更多信息,请参阅 Alarm Attachments

 
action_zoom_plus_stroke

Remove attachment

Click to remove the selected attachment from the alarm decoration rule.

 
action_zoom_plus_stroke

Navigate to 

Click to open the attachment that is selected in the attachment list.

Type

View the object type of the attachment.

Name

View the name of the attachment.

Display on alarm

Select to display the attachment when the alarm is going from Normal to Alarm state. 

Path

View the path of the attachment.

  • Alarm Functions
  • Alarm Decoration
  • Create Object Dialog – Naming the Object Page
  • Create Alarm Wizard – Presentation Page
  • Create Alarm Wizard – User Action Page