earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 1.9
12/14/2016

Create Alarm Wizard – Presentation Page

Use the Presentation page to configure the presentation settings of the alarm.

 
action_zoom_plus_stroke Presentation page
Figure: Presentation page

Table: Presentation Page

Component

Description

Above upper limit message

​Type the message to display when the variable exceeds the upper limit of the alarm.

Below lower limit message

​Type the message to display when the variable falls below the lower limit.

Alarm message

Type the message to display when the alarm is in Alarm state.

For more information, see Alarm Messages .

Reset message

​Type the message to display when the alarm is reset.

Category

​Enter the category that the alarm belongs to.

Prefix for alarm source name

Type a prefix that is added to the beginning of the source name property of an alarm record.

Above upper limit priority

​Enter the priority level of the alarm when the variable exceeds the upper limit.

Below lower limit priority

​Enter the priority level of the alarm when the variable falls below the lower limit.

Alarm priority

Enter the priority level of the alarm.

Reset priority

​Enter the priority level of the alarm when it is reset.

Same priority

Select to set all priorities to the same value.

Auto hide

Select to automatically hide the alarm in the Alarms pane or Alarm View.

Flashing alert

Select to make the alarm row flash in the Alarms pane and Alarm Views when the alarm is triggered.

Audible alert

Select to make the alert audible when the alarm is triggered.

Disable state-change logging

Select to prevent an alarm state change from creating an event.

  • Alarm Functions
  • Create Alarm Wizard – User Action Page
  • Create Alarm Wizard – Attachment Page
  • Create Object Wizard – Naming the Object Page
  • Alarm Substitution Codes
  • Alarm Messages