earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2023
2023/2/14

Create Alarm Wizard – Presentation Page

Use the Presentation page to configure the presentation settings of the alarm.

 
action_zoom_plus_stroke Presentation page
图: Presentation page

表格: Presentation Page

Component

Description

Above upper limit message

​Type the message to display when the variable exceeds the upper limit of the alarm.

Below lower limit message

​Type the message to display when the variable falls below the lower limit.

Alarm message

Type the message to display when the alarm is in Alarm state.

有关更多信息,请参阅 Alarm Messages .

Reset message

​Type the message to display when the alarm is reset.

有关更多信息,请参阅 Alarm Messages .

Category

​Enter the category the alarm belongs to.

有关更多信息,请参阅 Alarm Categories .

Category 2

Enter the second category the alarm belongs to.

有关更多信息,请参阅 Alarm Categories .

Prefix for alarm source name

Add a substitution code or type a prefix that is added to the beginning of the source name property of an alarm record.

有关更多信息,请参阅 Alarms Substitution Codes .

Above upper limit priority

​Enter the priority level of the alarm when the variable exceeds the upper limit.

有关更多信息,请参阅 Alarm Priority .

Below lower limit priority

​Enter the priority level of the alarm when the variable falls below the lower limit.

有关更多信息,请参阅 Alarm Priority .

Alarm priority

Enter the priority level of the alarm.

有关更多信息,请参阅 Alarm Priority .

Reset priority

​Enter the priority level of the alarm when it is reset.

有关更多信息,请参阅 Alarm Priority .

Same priority

Select to set all priorities to the same value.

有关更多信息,请参阅 Alarm Priority .

Auto hide

Select to automatically hide the alarm in the Alarms pane or Alarm View.

有关更多信息,请参阅 Alarm Decoration .

Flashing alert

Select to make the alarm row flash in the Alarms pane and Alarm Views when the alarm is triggered.

有关更多信息,请参阅 Alarm Decoration .

Audible alert

Select to make the alert audible when the alarm is triggered.

有关更多信息,请参阅 Alarm Decoration .

Custom audio

Enter the path to the custom audio file you to play when the alarm is triggered.

有关更多信息,请参阅 Custom Audible Alarm Alerts .

Disable state-change logging

Select to prevent an alarm state change from creating an event.

有关更多信息,请参阅 报警状态更改记录 .

  • Alarm Functions
  • Create Alarm Wizard – User Action Page
  • Create Alarm Wizard – Attachment Page
  • Create Object Dialog – Naming the Object Page
  • Alarms Substitution Codes
  • Alarm Messages
  • Alarm Categories
  • Alarm Priority
  • Alarm Decoration
  • Custom Audible Alarm Alerts
  • 报警状态更改记录