Funkcje: Alarmy
Wersja produktu: 3.2, 3.3, 2022
2022-08-16

Create Alarm Wizard – User Action Page

Use the User actions page to force a user to actions that are connected to the alarm.

 
action_zoom_plus_stroke User Action page
Rysunek: User Action page

Tabela: User Action Page

Component

Description

Acknowledgement type

​Select the type of acknowledgement for the alarm.

Więcej informacji zawiera Acknowledgements .

Cause note group

​Enter the cause note group that is used by the alarm.

Action note group

​Enter the action note group that is used by the alarm.

Checklist

​Enter the checklist that belongs to the alarm.

Required user action

​Select what actions the user has to perform when any of the listed events occur.

  • Alarm Functions
  • Create Object Dialog – Naming the Object Page
  • Create Alarm Wizard – Presentation Page
  • Create Alarm Wizard – Attachment Page
  • Comments
  • Cause Notes
  • Action Notes
  • Checklists
  • Hide and Disable
  • Alarm Assignments