earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WorkStation, Project Configuration Server
Functionalities: Basic Functionality
Product version: 1.8
10/13/2016

Create Object Wizard – Naming the Object Page

Use the Naming the object page to set the basic properties for the object. For objects with several types, you also select the object type.

 
action_zoom_plus_stroke Naming the object page
Figure: Naming the object page

Table: Naming the Object Page

Component

Description

(Object type list)

Select the type of object you want to create. For more information, see Building Operation Objects .

Name

Type the name of the object. For more information, see Object Names .

Prefix

Type a label that is added in front of the object name. For more information, see Suffix and Prefix .

Suffix

Type a label that is added after the object name. For more information, see Suffix and Prefix .

Path

Enter the path to the location in the System Tree where you want to create the object. By default, the path to the selected folder or object in the System Tree is displayed.

Description

Type a description that explains what the object is used for.

  • Building Operation Objects
  • Object Names
  • Suffix and Prefix