earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos WorkStation
Funcionalidades: Funcionalidad básica
Versión del producto: 3.2, 3.3, 2022, 2023
17/11/2020

Create Object Dialog – Naming the Object Page

Use the Create Object dialog to create and edit an object.

 
action_zoom_plus_stroke Create object dialog
Figura: Create object dialog

Tabla: Create Object Dialog

Component

Description

(Object type list)

Select the type of object you want to create. Para obtener más información, consulte EcoStruxure Building Operation Objects .

Name

Type the name of the object. Para obtener más información, consulte Object Names .

Prefix

Type a label that is added in front of the object name. Para obtener más información, consulte Suffix and Prefix .

Suffix

Type a label that is added after the object name. Para obtener más información, consulte Suffix and Prefix .

Path

Enter the path to the location in the System Tree where you want to create the object. By default, the path to the selected folder or object in the System Tree is displayed.

Description

Type a description that explains what the object is used for.

Next

Click to use the wizard when you create the object.

Create and edit

Click to create the object. This option closes the Create object dialog and navigates to the object.

Create

Click to create the object and close the Create object dialog

  • EcoStruxure Building Operation Objects
  • Object Names
  • Naming Convention
  • Suffix and Prefix