Use the Naming the object page to set the basic properties for the object. For objects with several types, you also select the object type.
Component |
Description |
(Object type list) |
Select the type of object you want to create. 有关更多信息,请参阅 EcoStruxure Building Operation Objects . |
Name |
Type the name of the object. 有关更多信息,请参阅 Object Names . |
Prefix |
Type a label that is added in front of the object name. 有关更多信息,请参阅 Suffix and Prefix . |
Suffix |
Type a label that is added after the object name. 有关更多信息,请参阅 Suffix and Prefix . |
Path |
Enter the path to the location in the System Tree where you want to create the object. By default, the path to the selected folder or object in the System Tree is displayed. |
Description |
Type a description that explains what the object is used for. |