earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Сигналы тревоги
Версия продукта: 2024, 7.0
02.12.2024

No Acknowledgement

When you select the acknowledgment type No acknowledgement, the triggered alarm returns to normal state and disappears from the alarm view when the monitored variable no longer meets the criteria to trigger the alarm. You select this user action when the user only needs to see a status and does not need to take any action on the alarm, for example, to see if a space is occupied or not.

 
action_zoom_plus_stroke No acknowledgement loop where the alarm does not have to be acknowledged before the alarm returns to normal state.
Рисунок: No acknowledgement loop where the alarm does not have to be acknowledged before the alarm returns to normal state.

The user can acknowledge the alarm in the alarm view to let other users know that the alarm has been noted. The acknowledgment is optional and the alarm does not require an acknowledgement to return to normal state.

 
action_zoom_plus_stroke No acknowledgement loop where the alarm is acknowledged before it returns to normal state.
Рисунок: No acknowledgement loop where the alarm is acknowledged before it returns to normal state.
  • Acknowledgements
  • Alarm Functions
  • Alarm States
  • Alarms Overview
  • Create Alarm Wizard – User Action Page
  • Configuring the Acknowledgement Type of an Alarm
  • Alarm Handling Issues