earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1
2018/10/26

Non-Validated Programs Search Example

​You want to find the programs that are not validated in your system. So you search for all programs that have validation set to None or Failed.

You only want to search in University X, so you ​right-click University X and then click Search. You want to find all programs that are not validated regardless of their names. The Search box cannot be empty and you want to find all programs regardless of their names so you should enter an asterisk (*).

 
action_zoom_plus_stroke  Search View when you have entered an asterisk (*) that finds all objects in University X
图: Search View when you have entered an asterisk (*) that finds all objects in University X

​To narrow your search so that only Script or Function Block programs are found, you should add Function Block Program and Script Program in the Select Types dialog box.

 
action_zoom_plus_stroke Select Types dialog box when all object types of the categories Function Block Program and Script Program are selected
图: Select Types dialog box when all object types of the categories Function Block Program and Script Program are selected

Then you select the conditions for the search in the Select Conditions dialog box. We only want to find non-validated programs. Therefore, we choose Validation from the Add condition list, and then we select None and Failed, and click OK.

 
action_zoom_plus_stroke Validation conditions None and Failed selected in the Select Conditions dialog box
图: Validation conditions None and Failed selected in the Select Conditions dialog box

Then we perform the search.

 
action_zoom_plus_stroke Search result for all programs in University X that are not validated successfully
图: Search result for all programs in University X that are not validated successfully

To be able to use the search again without going through all the settings once more we save the search with the name “Non-Validated Program Search”.

  • Search Overview
  • Search
  • Search View
  • Select Folder Dialog Box
  • Select Types Dialog Box
  • Select Conditions Dialog Box
  • Searching for Objects or Properties
  • Saving a Search