earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: WebReports
Funktionaliteter: Rapporter
Produktversion: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
2021-12-16

Unit Configuration Errors Report

The Unit Configuration Errors report is a WebReports Diagnostics report that enables you to identify which extended trend logs (if any) have incorrectly configured energy units. The report also contains the names of energy meters that are associated with the extended trend logs, and the system point that is logged. In addition, the Unit Configuration Errors report states whether the units are incorrectly set (that is, the wrong type of unit), or simply that no unit at all is configured.

The Unit Configuration Errors report is contained in the WebReports Diagnostics folder in the Reports folder.

Tabell: Unit Configuration Errors Input Parameters

Input Parameters

Description

None

The Unit Configuration Errors report does not prompt for filtering criteria.

  • WebReports Diagnostic Reports
  • Factory Supplied Reports