earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 3.2
10/15/2020

SmartX Server Replacement Using Restore Workflow

Use the workflow to duplicate the SmartX server from a backup set.

 
action_zoom_plus_stroke Duplicate SmartX server using restore flowchart
Figure: Duplicate SmartX server using restore flowchart
Copy SmartX server Backup Set to WorkStation

Save the most current backup set of the SmartX server that you want to replace to WorkStation.

For more information, see Saving a SmartX Server Backup Set to Another Location .

Add new SmartX server to network and configure communication settings

Add the new SmartX server to the network and configure the IP address.

For more information, see Configuring a SmartX Server to Use DHCP .

For more information, see Configuring the SmartX Server IP Address .

Log on to SmartX server using WorkStation

For more information, see Logging on to WorkStation as an EcoStruxure Building Operation User .

Import backup set

Import the backup set to the new SmartX server.

For more information, see Importing a Backup Set to SmartX Server .

Restore new SmartX server using the imported Backup Set

Restore the new SmartX server using the imported backup set.

For more information, see Restoring the EcoStruxure BMS Server .

Tip:

If the SmartX server does not go online, you can manually recreate the SmartX server or restore the connections between the Enterprise Server and the SmartX server. For more information, see SmartX Server Remains Offline After Restore .

The Restore process automatically renames the SmartX server and specifies the objects and properties that the SmartX server uses to reestablish links and go online.

  • Restore
  • SmartX Server Replacement Using Restore
  • Backup Sets
  • Saving a SmartX Server Backup Set to Another Location
  • Configuring a SmartX Server to Use DHCP
  • Configuring the SmartX Server IP Address
  • Logging on to WorkStation as an EcoStruxure Building Operation User
  • Importing a Backup Set to SmartX Server
  • Restoring the EcoStruxure BMS Server
  • SmartX Server Remains Offline After Restore