earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-C, AS-B, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 1.8, 1.9
2017/4/5

SmartStruxure Server Device Replacement Using Restore Workflow

Use the workflow to duplicate the SmartStruxure server device from a backup set.

 
action_zoom_plus_stroke Duplicate SmartStruxure server device using restore flowchart
图: Duplicate SmartStruxure server device using restore flowchart
Copy SmartStruxure server device Backup Set to WorkStation

Save the most current backup set of the SmartStruxure server device that you want to replace to WorkStation.

有关更多信息,请参阅 Saving a SmartStruxure Server Device Backup Set to Another Location .

Add new SmartStruxure server device to network and configure communication settings

Add the new SmartStruxure server device to the network and configure the IP address.

有关更多信息,请参阅 Configuring a SmartStruxure Server Device to Use DHCP .

有关更多信息,请参阅 Setting the SmartStruxure Server Device IP Address .

Log on to SmartStruxure server device using WorkStation

有关更多信息,请参阅 以楼宇管理系统用户身份登录工作站 .

Import backup set

Import the backup set to the new SmartStruxure server device.

有关更多信息,请参阅 Importing a Backup Set to SmartStruxure Server Device .

Restore new SmartStruxure server device using the imported Backup Set

Restore the new SmartStruxure server device using the imported backup set.

有关更多信息,请参阅 Restoring the SmartStruxure Server .

提示:

If the SmartStruxure server device does not go online, you can manually recreate the SmartStruxure server device or restore the connections between the Enterprise Server and the SmartStruxure server device. 有关更多信息,请参阅 SmartStruxure Server Device Remains Offline After Restore .

The Restore process automatically renames the SmartStruxure server device and specifies the objects and properties that the SmartStruxure server device uses to reestablish links and go online.

  • Restore
  • SmartStruxure Server Device Replacement Using Restore
  • Backup Sets
  • Saving a SmartStruxure Server Device Backup Set to Another Location
  • Configuring a SmartStruxure Server Device to Use DHCP
  • Setting the SmartStruxure Server Device IP Address
  • 以楼宇管理系统用户身份登录工作站
  • Importing a Backup Set to SmartStruxure Server Device
  • Restoring the SmartStruxure Server
  • SmartStruxure Server Device Remains Offline After Restore