earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server
功能: 基本功能
产品版本: 1.8
2016/6/10

Object Names

All objects in the Building Operation database has to have a name. Building Operation is case-sensitive and differentiates between upper and lowercase characters. ​Two objects cannot be named in the same way in the same folder even if the objects are of different types.  For example, you cannot create an alarm named Building A and a graphic named Building A in the same folder. However, if you name the graphic Building a, with a lowercase a, you can create it in the same folder as the alarm object Building A.

​The following characters are not allowed in object names in Building Operation.

  • /

  • "

  • ?

  • *

  • ~

  • <

  • >

  • |

  • White space is not allowed in the beginning or the end of an objects name.

  • . (period) is not allowed in the beginning or the end of an objects name.

​There is no limitation of how many characters an object name can have. However, some field devices retain their character limitations when they are added to Building Operation database.

  • Object Properties
  • Language Packages
  • Regional and Language Overview