Funktionen: Basisfunktionalität
Produktversion: 3.2, 3.3, 2022
15.10.2020

EcoStruxure Building Operation Objects

arrow1_rotationObject Names arrow1_rotationObject Properties arrow1_rotationContent Types arrow1_rotationList View Features

The EcoStruxure Building Operation database is based on objects. Some objects are created when the database in installed, others are created by the engineer. Depending on the object type and your permissions, you can configure objects in a many different way.

Objects that are relevant for the user are presented in the System Tree pane and in the List View. To ease recognition of objects, every object type is represented by an icon.

Object Names

All objects in the EcoStruxure Building Operation database have to have a name. The EcoStruxure Building Operation objects are case-sensitive and differentiates between upper and lowercase characters. ​

Für weitere Informationen siehe Object Names .

Object Properties

Every object in the EcoStruxure Building Operation database has a number of different properties. Properties can be of two different types: read only and read/write. Read only properties are dimmed and cannot be changed. Read/write properties can be changed.

Für weitere Informationen siehe Object Properties .

Content Types

Content types are predefined layouts that you save to reuse for specific types of folders or container objects.

Für weitere Informationen siehe Content Types .

List View Features

You use the List View to view, manage, and mass edit objects in the EcoStruxure Building Operation database.

Für weitere Informationen siehe List View Features .

  • WorkStation
  • Object Names
  • Object Properties
  • Content Types
  • List View Features
  • Basic Functionality Icons in the System Tree Pane
  • Systembaumfenster
  • Listenansicht
  • Objekte sortieren und gruppieren
  • Adding and Removing Columns
  • Die Spaltenbreite an den Inhalt anpassen