earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Basic Functionality
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
5/18/2018

Opening a Document

You open, edit, and save documents stored on an EcoStruxure BMS server using the default editor associated with the file type. For example, the Notepad editor opens a text file.

Show More
action_close

You can open documents stored on a StruxureWare Server using the default program associated with the file type. For example, a txt-file opens Notepad and a ppt-file opens PowerPoint.

When you click on the document in WorkStation, the document is opened using the associated editor or viewer. For example, a txt-file is opens Notepad, a xsl-file opens Excel. The editor of viewer associated with the file type has to be installed on the same computer as WorkStation.

The documents can be edited and then saved in Building Operation again.

To open a document
  1. In WorkStation, in the System Tree pane, click the document.

  2. When the editor opens the document, you can view or modify the file.

  3. When finished, save and close the document.

  • How Documents Work
  • Documents Overview