Produits : WorkStation
Fonctionnalités : Fonctionnalité de base
Version produit : 2024, 7.0
02/12/2024

Opening a Document

You open, edit, and save documents stored on an EcoStruxure BMS server using the default editor associated with the file type. For example, the Notepad editor opens a text file.

Afficher plus
action_close

You can open documents stored on an EcoStruxure BMS server using the default program associated with the file type. For example, a txt-file opens Notepad and a ppt-file opens PowerPoint.

You can edit the documents and then save them again using WorkStation. You cannot edit and save documents using WebStation.

Déclaration

When you log off or are automatically logged off, any unsaved changes in the document are not saved in the database. Make sure that you save changes in open documents frequently.

To open a document
  1. In WorkStation, in the System Tree pane, click the document.

  2. When the editor opens the document, you can view or modify the file.

  3. When finished, save and close the document.

  • How Documents Work
  • Documents Overview