earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WorkStation
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-05-18

Opening a Document

You open, edit, and save documents stored on an EcoStruxure BMS server using the default editor associated with the file type. For example, the Notepad editor opens a text file.

Pokaż więcej
action_close

You can open documents stored on an EcoStruxure BMS server using the default program associated with the file type. For example, a txt-file opens Notepad and a ppt-file opens PowerPoint.

You can edit the documents and then save them again using WorkStation. You cannot edit and save documents using WebStation.

Uwaga

When you log off or are automatically logged off, any unsaved changes in the document are not saved in the database. Make sure that you save changes in open documents frequently.

To open a document
  1. In WorkStation, in the System Tree pane, click the document.

  2. When the editor opens the document, you can view or modify the file.

  3. When finished, save and close the document.

  • How Documents Work
  • Documents Overview