earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Функции: Тренды
Версия продукта: 2024, 7.0
02.12.2024

Viewing a Trend Log in a Temporary Trend Chart

You open a trend log as a temporary trend chart to view the recorded values graphically. When you close the temporary trend chart, the chart is not saved.

Показать больше
action_close

​To display a trend log without creating a new trend log list or trend chart, the trend log can be displayed in a temporary list or chart.

 
action_zoom_plus_stroke Trend log displayed in a temporary trend log list and temporary trend chart
Рисунок: Trend log displayed in a temporary trend log list and temporary trend chart
Примечание

You have to manually refresh the trend log list.

To view a trend log in a temporary trend chart
  1. In WorkStation, in the System Tree pane, select the folder or EcoStruxure BMS server where the trend log is located.

  2. Select the trend log you want to open as a temporary trend chart.

  3. On the Actions menu, point to the View submenu and then click In Trend Chart .

The temporary trend chart is displayed in the work area under a generic name.

  • Temporary Trend Charts
  • Temporary Trend Log Lists
  • Saving the Trend Chart Settings
  • Trend Chart View