Productos Enterprise Central, Enterprise Server, Software Administrator
Funcionalidades: Ingeniería
Versión del producto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
18/05/2018

Viewing the Enterprise Server or Enterprise Central System Log

You view logged server events in the Enterprise Server or Enterprise Central system log to troubleshoot server problems that are traced to the Enterprise Server or Enterprise Central.

Mostrar más
action_close

The Enterprise Server and Enterprise Central System logs contain events logged by the Enterprise Server or Enterprise Central. Examples of logged events are startup sequence, port settings, failures, run time, and current server status.

To view the Enterprise Server or Enterprise Central system log
  1. In Software Administrator, click the Enterprise Server or Enterprise Central tab.

  2. In the System box, view the events in the system log.

  3. Click OK .

  • ​Enterprise Server does not Start
  • Enterprise Server and Enterprise Central System Logs
  • Software Administrator
  • Software Administrator – Enterprise Server View
  • Software Administrator – Enterprise Central View
  • Starting Software Administrator