earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Como

Como


Produtos: WorkStation
Funcionalidades: Funcionalidade básica
Versão do produto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
16-11-2018

Abrir uma vista de eventos específicos de objeto

Pode ver todos os eventos relacionados com um objeto específico ou um ramo específico.

Nota

O filtro padrão específico de objeto apenas pode reduzir o que está a ser apresentado na vista de evento.

Mostrar mais
action_close

You can style certain events to bring out those that are of more interest than other events listed in the Events pane and Event Views. To style a specific event, you first have to create a condition that is associated with the events you want to style. An event can be styled with a unique background color, font, and font color.

For example, you can style all events where an alarm is acknowledged. To separate this event from others you configure, change the background color to dark green and the font color to white. All other events have the default style which is a white background and black font color.

If an event fulfills the condition criteria in more than one of the configured event criteria, it is the event style with highest priority in the Events View Style dialog box that is applied to the event.

Events styling does not apply to WebStation and does not affect the events in WebStation.

Event View standard filter and layout

A standard layout defines the columns that are included in the Alarms pane, Events pane, Alarm View, or Event View, the order in which they are displayed, whether or not the alarms or events are grouped in any way and whether they are displayed in an ascending or descending order. A standard filter defines the conditions that have to be met before the alarms or events are displayed in the pane or a View. The standard layout and filter is saved for the pane or View to which you made the changes. The standard layout and filter is displayed for all users of the the EcoStruxure BMS.

Para mais informações, consulte Alarm View and Event View Standard Filter and Layout .

Para abrir uma vista de eventos específica de objeto
  1. No painel árvores de sistema , selecione o objeto para o qual pretende ver os eventos.

  2. No menu Ações , aponte para Vista e depois clique em Eventos ou Eventos neste ramo .

  • How Events Work
  • Painel de eventos e vista de eventos
  • Barra de ferramentas de painel de eventos e vista de eventos
  • Actions Menu