earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funkcje: Trendy
Wersja produktu: 3.2, 3.3, 2022
2021-07-22

Editing the Trend Chart Settings

You configure the scale of the trend chart axes, the presentation of series, and the calculation method to make it easier to interpret the series, representing the trend log records, in the trend chart.

Pokaż więcej
action_close

The x-axis of the trend chart represents time. The time span of the axis can be set with a fixed start and end time or with an end time relative to the present time. The axis can be quick-scaled to show the last hour, last day, last month, or last year​.

 
action_zoom_plus_stroke Absolute time span and relative time span, schematic
Rysunek: Absolute time span and relative time span, schematic

The y-axis refers to the measurement unit that the variable represents. The scale of the y-axis can be set manually or by auto scale. You can configure the trend chart to present series on one y-axis or two y-axes, one to the left and one to the right. Use two y-axes to present series with different ranges in the same trend chart.

 
action_zoom_plus_stroke One y-axis and two y-axes, schematic
Rysunek: One y-axis and two y-axes, schematic

To make reading easier, grid lines can be shown in the trend chart. Grid lines can be shown in both the x- and y-direction, independent of each other.

 
action_zoom_plus_stroke Grid lines, schematic
Rysunek: Grid lines, schematic

To edit the trend chart settings
  1. In WorkStation, in the System Tree pane, select the trend chart.

  2. On the Trend Chart toolbar, click Open trend chart settings button

     
    action_zoom_plus_stroke
    .

  3. In the Trend Chart Settings dialog box, edit the trend chart settings.

  4. Click OK .

  • Trend Chart Axes
  • Trend Chart Settings Dialog Box – Axes Tab
  • Trend Chart Event Icons
  • Trend Chart View