earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Gestión de usuarios
Versión del producto: 3.2, 3.3, 2022
15/10/2020

Pane Properties

Use the Pane properties to configure the settings of the pane.

 
action_zoom_plus_stroke Pane properties
Figura: Pane properties

Tabla: Pane Properties

Component

Description

Show toolbar

Select Yes to show the toolbars for the pane component.

Default dock position

Select where to place the pane in the workspace.

Default visibility

Select Hidden to hide the pane.

Dipslay name

Type the pane name that is to be displayed. Display name is available only in Workstation.

Initial path

Enter the path to the pane component.

  • Workspace Management
  • General Information Properties – Basic Tab