Use the Panel Configuration page to add components to the panel.
Component |
Description |
![]() |
Add Click to add a new component to the panel. For more information, see Create Object Wizard – Naming the Object Page . |
![]() |
Edit Click to edit the properties of a component. For more information, see Pane Properties . |
![]() |
Remove Click to remove a component from the panel. |
Work area initial path |
Click to enter the path for the Work area component. |
Show toolbars |
Select Yes to show the toolbars for the Work area component. |