Funkcje: Zarządzanie użytkownikiem
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Panel Wizard – Panel Configuration Page

Use the Panel Configuration page to add components to the panel.

 
action_zoom_plus_stroke Panel configuration page
Rysunek: Panel configuration page

Tabela: Panel Configuration Page

Component

Description

 
action_zoom_plus_stroke

Add

Click to add a new component to the panel. Więcej informacji zawiera Create Object Dialog – Naming the Object Page .

 
action_zoom_plus_stroke

Edit

Click to edit the properties of a component. Więcej informacji zawiera Pane Properties .

 
action_zoom_plus_stroke

Remove

Click to remove a component from the panel.

Work area initial path

Click to enter the path for the Work area component.

Show toolbars

Select Yes to show the toolbars for the Work area component.

  • Panel Components
  • Panel Properties
  • Create Object Dialog – Naming the Object Page