There are two LEDs on the front panel of the PS-24V. The LEDs indicate status for input and output power.
Function |
Color |
Main power |
Green |
Status |
Green/red |
The Main Power LED indicates status for input power. The Main Power LED indicates the condition according to the following table.
LED Patterns |
Condition |
Green, constant |
Input power |
No light |
No input power |
The Status LED on the front of the SmartStruxure devices changes color and flashes to indicate the status of the device.
Für weitere Informationen siehe Status LEDs .