earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos PS-24 V
Funcionalidades: Hardware
Versión del producto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
18/05/2018

Power Supply PS-24V LEDs

arrow1_rotationMain Power LED arrow1_rotationStatus LED

There are two LEDs on the front panel of the PS-24V. The LEDs indicate status for input and output power.

 
action_zoom_plus_stroke ​PS-24V power supply LEDs
Figura: ​PS-24V power supply LEDs

Tabla: Power Supply PS-24V LEDs

Function

Color

Main power

Green

Status

Green/red

Main Power LED

The Main Power LED indicates status for input power. The Main Power LED indicates the condition.

Tabla: Main Power LED Patterns

LED Patterns

Condition

Green, constant

Input power

No light

No input power

Status LED

The PS-24V power supply Status LED indicates the condition of the device.

Tabla: Power Supply Status LED Patterns

LED Patterns

Condition

Green, constant

Output voltage and load OK

Red/green, flashing

Output slightly overloaded

Red, constant

Output overloaded

No light

No input power

  • PS-24V Power Supplies
  • Status LEDs
  • Power Supply Overload