earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 本地化
产品版本: 2.0, 2.1, 3.0, 3.1
2022/5/30

Precision Format

​Values in the EcoStruxure Building Operation software are stored in the EcoStruxure Building Operation database with all input decimals. If a stored value consists of more decimals than the operating system is defined to display, the value is rounded off according to the operating system settings before it is displayed in WorkStation.

For example, you enter the length 6.5282 m (21.4179 ft) to a variable in Building Operation. When you press Enter or OK, the value changes to 6.53 m (21.41 ft). This becouse of your operating system, in this example, is defined to display only two decimals The input value 6.5282 m (21.4179 ft) is stored in the Building Operation database but is round off to 6.53 m (21.41 ft) when it is displayed.

注释:
  • The rounded value is only a display value and is not used by Building Operation in calculations or other operations.

If an integer value exceeds 12 digits (10 12 ), both positive and negative numbers, WorkStation displays the value in scientific notation. The number of digits for a decimal number before it is displayed in scientific notation is decided by the regional settings of the operating system settings where WorkStation is installed.

  • Value Presentation
  • Regional and Language Overview
  • Configuring Regional Settings