功能: 用户管理
产品版本: 1.8
2016/10/13

Predefined Workspaces

​Some workspace layouts are included in the Building Operation main installation and cannot be deleted or edited. Those workspaces are located in the local domain of the SmartStruxure server.

表格: Predefined Workspaces

Predefined Workspaces

Description

System Default Workspace

The System Default Workspace displays if there is no workspace available for users that log on to WorkStation. For example, Building Operation uses this workspace when the user account group the user belongs to has no workspaces associated with it, or the user's default workspace is deleted by the system administrator.

Administration Workspace​

The Administration Workspace displays ​if there is no other workspace available for administrators logging on to WorkStation. The purpose of the Administration workspace is to ensure that users with administrator rights always have access to all properties and functions.

Engineering Workspace

​In addition to the System Default Workspace and Administration Workspace that are installed when Building Operation is installed, you also have the option to install a predefined engineering workspace. The purpose of the Engineering workspace is to configure WorkStation, view events and alarms.​

  • 切换工作区
  • 选择默认工作区
  • User Account Management Overview
  • Workspace Management