earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Como

Como


Produtos: AO-8, AO-V-8, AS-B, DI-16, DO-FA-12, DO-FC-8, AS-P, Project Configuration Tool, RTD-DI-16, UI-16, UI-8/AO-4, UI-8/AO-V-4, UI-8/DO-FC-4
Funcionalidades: Comunicação I/O, Hardware
Versão do produto: 3.3, 2022, 2023, 2024
24-02-2022

Printing a Label to Identify I/O Channels

You print labels to identify I/O channels on the placard of an I/O module much the same way you label circuits on an electrical panel. You accept the default names for the I/O point labels or customize the I/O point names for your own application.

Nota

If a Module ID is Null, you cannot print the label. If a channel is Null, the I/O point labels do not display in the Print IO Module Labels dialog box.

To print a label to identify I/O channels
  1. In WorkStation, in the System Tree pane, expand the IO Bus on an automation server.

  2. In the List View , right-click the Central IO module, AS-B onboard IO, the entire IO Bus folder, or multiple Central IO modules.

  3. Click Print IO module labels .

  4. In the Print IO Module Labels dialog box, select Blank Label Text to print labels with only the channel number with no additional label text.

    Nota

    The label text prints in red if the text is too long to fit on the label.

  5. In the Paper Type box, select a paper type.

  6. Click Print to print the I/O module label or Save to save any changes to the point’s label text property.

  7. For AS-B onboard I/O, cut along the dotted lines and fold the label along the fold edge to fit on the placard.

The label is properly sized to fit on the placard of the I/O module.

  • Central IO Modules Overview
  • Print Central IO Module Labels Dialog Box
  • Printing a Wiring List for the I/O Bus